6/6/2023 7:54 AM | |
Joined: 3/8/2017 Last visit: 2/13/2024 Posts: 15 Rating: (3) |
Hi, in order to reduce the need for big data requests there is one think you can do that I know of. In the Data Service it is possible to create aggregations which are pre-calculated. For example you want a mean temperature in an hourly cycle which otherwise gets checked every second. This would reduce the requested data by a factor of 3600. In order to create this pre-calculated aggregation you have to open the DataService UI and edit the variable under the aggregation tab. Of course this is not a dynamic solution but might already help you. You can find further information in the Data Service documentation v1.6 under "8.1 adding a variable" |
Last edited by: Jen_Moderator at: 06/06/2023 09:37:12Link optimized. |
|
Follow us on