7/4/2024 8:48 AM | |
Joined: 7/3/2024 Last visit: 7/17/2024 Posts: 2 Rating: (0) |
Hello, We are using Tia portal v19, and still very green behind the ears. we're wondering if it is recommended or if at all possible to use one single SVGHMI for the visual graphics in the overview screen. The file size is about 1,7Mb Here the SVGHMI with only the dynamics for fill levels of silos:
AttachmentSVGHMI.txt (3 Downloads) |
Last edited by: marb121 at: 07/04/2024 09:31:56Last edited by: Wit_Moderator at: 07/05/2024 12:30:45Log added as txt-file |
|
7/4/2024 10:10 AM | |
Joined: 7/3/2024 Last visit: 7/17/2024 Posts: 2 Rating: (0) |
Thanks for your fast reply. I figured that using the transform attr on text was not a good idea. Kind regards. |
Follow us on