8/2/2024 12:03 PM | |
Joined: 7/11/2024 Last visit: 9/26/2024 Posts: 43 Rating: (3) |
Hi vlade200 Does it also happen if you create a test project?In that case, it seems that the WinCC installation is corrupted and it would be interesting to reinstall it again. I understand that when you say that you reset the PC you mean to restart it. If it only happens with that project in question I would try, first, to delete the DCF as you can check here: Update configuration file of the WinCC project (delete DCF) Good luck! |
If this comment was helpful, be sure to rate it! |
|
9/11/2024 9:45 AM | |
Joined: 8/3/2009 Last visit: 9/27/2024 Posts: 13794 Rating: (1741)
|
Hello vlade200 Windows in the Home edition is not released for WinCC V8 I know that also in older Versions the Home Version has often caused trouble with WinCC. Use on eof the released OS for WinCC V8: https://support.industry.siemens.com/cs/de/en/view/64847781 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on