6/8/2024 9:02 PM | |
Joined: 12/30/2019 Last visit: 9/18/2025 Posts: 27 Rating:
|
I have a question related to this. Would it be possible to send the run/stop command to the webserver from a third party application through an HTTP Post Command. This removes the need for me to login to the Siemens Webserver to run or stop the PLC. I examined the traffic sent on wireshark when the stop/run button is clicked on the webserver and it looks like it's a bunch of HTTP Post commands to run/stop the PLC What I need help with would be how to craft the HTTP Request required Has anyone done something like this? ------------------------------------------------------------------------------------------ |
Last edited by: Oladimgba at: 06/08/2024 21:04:03Last edited by: Jen_Moderator at: 06/10/2024 08:52:59New subject after splitting |
|
9/16/2024 2:39 PM | |
Joined: 3/23/2020 Last visit: 3/20/2025 Posts: 10 Rating:
|
Hello I have come across this discussion, have you figured out the start/stop of the PLC using the POST method ? I am doing it in Openness but I dont like that even openness does not have any proper method implemented for the Start/Stop of the PLC. In Openness it is done through download procedure. So I would very much use the same usecase as you have mentioned. To simply call some endpoint with POST method to be able to Start/Stop the PLC.
|
Last edited by: vformanek at: 09/16/2024 14:39:25Last edited by: vformanek at: 09/16/2024 14:39:54 |
|
9/18/2024 6:34 AM | |
Joined: 10/7/2005 Last visit: 9/21/2025 Posts: 3049 Rating:
|
The API of the S7-1500 Webserver does - for better or worse - cater for this and chapter 5.7 of the S7-1500 Webserver manual has the details. |
Cheers |
|
This contribution was helpful to
3 thankful Users |
Follow us on