9/17/2024 6:54 AM | |
Joined: 5/6/2022 Last visit: 10/18/2024 Posts: 470 Rating: (94) |
Hi AutoGen_6034314, In this case we need more information to see if we can give you a hand. Can you tell us exactly which version of WinCC you have installed and the Windows version of the PC? When you try to open the project, do you get a specific error or nothing at all, does it only happen with one project or does it happen with all projects you create or try to open? Best regards!
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on