9/27/2024 12:17 PM | |
Joined: 10/17/2023 Last visit: 9/27/2024 Posts: 1 Rating: (0) |
Dear Forum Members, Version: Unified V19 Browser: Chrome Goal: start simulation --- Errors in TraceViewer: Project validation failed! Detected high level error (for details see following info traces): The runtime is running, operation expects stopped runtime (22) Attempted to stop runtime, while there's still another service created! CC_EventHandler::disconnect: current state for disconnect: %d %d %d %d %d [0, 0, 0, 1, 0] Precondition 'CheckLanguage(filterLang)' failed! (Hmi::QF::ActiveAlarmSubscriptionHandler::Subscribe) dai is NULL Unexpected state, CReadCallback, handle_result, error -9204590179157540888 Cid=,318 Oid=, 0x2 CHmiRuntime::Could not start project - project name missing in CContextStore! --- Result: simulation running but "site cannot be reached ... ERR_CONNECTION_RESET" Attempts but same error:
Where is the CHmiRuntime folder? Sounds something is wrong there. I assume it's C:\ProgramData\SCADAProjects but not sure How do you properly "rebuild runtime/project"? Maybe unrelated but connecting to WinCC SQL server through SSMS also showed no file. Did I miss some configuration? What else can be done |
9/27/2024 1:53 PM | |
Joined: 11/13/2018 Last visit: 9/27/2024 Posts: 28 Rating: (4) |
Hi AutoGen_6269199, I think it's best to create an SR for this. Afterwards, can you post what they said please? |
Follow us on