10/8/2024 1:34 PM | |
Joined: 5/5/2021 Last visit: 10/16/2024 Posts: 5 Rating: (0) |
hello I am making small project with im360 and im361. They are both on separate power supply If power on im361 goes down it causes PLC to go to stop. I tried putting many OBs in but no help Is there a way to prevent PLC with im360 go to stop and require restart when im361 is powered off? Right now only solution is to manually restart CPU... Has anyone found a solution to this? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/08/2024 14:09:14New subject after splitting |
|
10/11/2024 7:44 AM | |
Joined: 7/19/2022 Last visit: 10/18/2024 Posts: 403 Rating: (65) |
Hello MichalWZeta, When loading OB86 (What should you watch out for with regard to subrack failure when programming the OB86?) the CPU still goes to STOP when the peripheral is disconnected? |
If this Information really helps, you could use the Rate function |
|
Follow us on