8/29/2005 3:33 PM | |
Joined: 8/10/2005 Last visit: 4/9/2024 Posts: 1486 Rating: (32)
|
You wrote: >> I use WinCC 5.0 SP2. Now I want to save a raw Datatype >> tag in external format, where ( eg: DB100.DW0 , Dw0 I >> select as raw Data ). Which format can I export out, csv >> sure not possible ? And how can I retrieve it back ?. >> Do I need to write Global Script in User Archive ? If I >> don't have User Archive license, is there any other >> method ? How's the code ? You have to split the rawdata tag inot internal tags and write these tags into a csv file with the attached FAQ. The other possibility would be to use UserArchiv, but there you will need a licence for this WinCC Option. ==>> http://support.automation.siemens.com/WW/view/en/71078 Best Regards Technical Support |
Follow us on