12/4/2020 10:28 AM | |
Posts: 198 Rating: (60) |
Hello LucaG_SFT, According to the SIMATIC BATCH COM API V9.0SP1 manual, the sample project link points to "Sample Application for SIMATIC BATCH COM API" which is available in this link: https://support.industry.siemens.com/cs/ww/en/view/92344632 Hence, the files available in this sample should work with the higher versions of SIMATIC Batch. Can you please elaborate which files are missing when you tried to find it? |
Last edited by: Jen_Moderator at: 12/04/2020 10:33:35Optimized link. |
|
12/4/2020 4:45 PM | |
Joined: 12/4/2019 Last visit: 6/13/2023 Posts: 6 Rating: (1) |
Hello TechnoBlaze, the sample project dates back to 2016, so when you select which version of the API to use for the communication you can select v8.2.0 at most (see attachment): I expected to have also v9.0.0 and v9.0.1, and that's why I asked for the latest version of the IPCS7_SBAPI_XLib.dll. Do you have any idea of where can I find or download that dll file? Thank You, Luca |
12/11/2020 10:45 AM | |
Posts: 198 Rating: (60) |
Hello Luca, As of now, there is no link to download the latest version (9.0 or 9.0.1) of the dll (Smiley tool). It was removed after Batch V8.2. Are you facing any functionality issues while using this dll with V9.0.0 or V9.0.1 or you have not tried it yet? Nevertheless, you may consider raising a technical support request with Siemens if you feel the newer dll is a must for your requirement. https://support.industry.siemens.com/tf/ww/en/header/supportrequest/ |
Last edited by: TechnoBlaze at: 12/11/2020 10:46:13 |
|
Follow us on