5/9/2012 10:03 PM | |
Posts: 20 Rating:
|
Hi everyone! Do you know if it is possible to configure a Sed2 with Starter??? |
5/11/2012 11:29 PM | |
Joined: 6/4/2008 Last visit: 8/16/2024 Posts: 1492 Rating:
|
Hi, in reply to your question, it is a definite NO The only possibility I know of is using the SED2 BOP or AOP to program. Starter & Scout can only be used with the Sinamics and Micromaster family of drives. Whilst the SED2 looks like a Micromaster, it is a building technologies drive and due to it's relatively small DC Bus capacitance, it cannot be used (very well) on Industrial supplies. In case you don't have manuals, I attach all the SED2 manuals I have. Regards, Graeme AttachmentSiemens-SED2-Manuals.zip (786 Downloads) |
This contribution was helpful to
2 thankful Users |
Follow us on