8/13/2024 7:48 AM | |
Joined: 12/14/2023 Last visit: 8/13/2024 Posts: 2 Rating: (0) |
Hello Siemens Experts, I have problem with IO_link type AL1302 FROM ifm company, this io link canot be reachable from my plc s7 1500. this is the message which i found in diagnostics status as follows :- The IO device specified in the detailed information has failed or is not present. Check whether the failure belongs to an intended maintenance intervention. Check whether the failure occurs once or is repeatedly coming/going. Check whether there are more device failures and locate the failed device(s) in the IOSystem topology. Regard special device types (e.g. I devices, IE-IE-IOC) Remedy: Check power supply, network wiring and connectors. The IO device cannot be detected on the network. Remedy: The device may not be seen by the PLC due to wiring problems, power-off of the device or device failure. Check wiring to the device, check whether the device is up and running. The IO device is reachable, but does not have a PROFINET device name or IP address. Use online access / update accessible devices, assign PROFINET device name or similar tools to check the PROFINET device name and the IP address of the IO device. please your valuable answer will be highly appreciated. regards, ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 08/13/2024 09:16:39New subject after splitting |
|
Follow us on