4/8/2015 12:36 PM | |
Joined: 6/10/2014 Last visit: 10/3/2023 Posts: 10 Rating: (0) |
Hi Ganes, do you know what's the direct link for the log files for the 1500 CPU, because I've tried that in the chapter 4.2.4 and it doesnt' work, and those I've found in other threads don't work either. Thanks in advance. |
4/20/2015 4:11 PM | |
Posts: 1 Rating: (0) |
Hi, I am very new in SPS Programming World. Thank you, the attached program works fine. How fast is it possible to log the Analog signals using S7-1200(s7-1214DC/DC/DC). Is it possible to log in every 20 milisecond (may be more less). I need to log as more as data in short time for some experiments. In the given program, i have used a pulse signal, it gives the trigger to write data. If i give the pulse at higher frequency, it cannot write properly. May be because of those BUSY flags? The cycling time of my program is less than 5 ms. Regards, Milan
|
11/15/2015 9:58 PM | |
Joined: 1/23/2013 Last visit: 8/10/2022 Posts: 226 Rating: (5) |
Hi how to implement the file names in the form 11/11/2015.csv 11/12/2015.csv .............??? |
11/16/2015 7:47 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (821) |
Hello, probably impossible due not correct chars -> / |
With best regards... |
|
1/29/2016 12:57 PM | |
Posts: 1 Rating: (0) |
Hi, I have error: " 8092 Source data log does not exist"., when i wont to create DataLogNewFile. What is this error? Thanks! |
Follow us on