10/1/2020 5:48 PM | |
Joined: 11/12/2019 Last visit: 3/23/2022 Posts: 2 Rating: (0) |
Hi, I am having trouble getting a recipe to download a git repository via ssh using kas-docker. The build fails with the error
kas-docker is invoked with --ssh-dir=/home/iain/.ssh
The comparison of ssh -vT run natively and in kas-docker is attached (key values are sanitised). My suspicion is that the kas-docker implementation is missing the key passphrase that I occasionally have to enter in the native environment. Has anyone managed to solve this problem already? Thanks, Iain Attachmentssh-accesses.zip (721 Downloads) |
Follow us on