7/31/2025 11:51 AM | |
Joined: 7/24/2025 Last visit: 8/17/2025 Posts: 26 Rating:
|
Hello qwazee thank you for your answer The logic of my code is: I1(Sensor) is connected to counter1, counter 1 is connected to math instruction and from math instruction is connected to analog comparator. I2 (sensor) 2 is connected to counter 2, counter 2 is connected to math instruction 2 and math instruction 2 is connected to analog comparator. The sensors are digital |
Last edited by: duma_calin145 at: 07/31/2025 11:51:40 |
|
7/31/2025 11:57 AM | |
Joined: 7/24/2025 Last visit: 8/17/2025 Posts: 26 Rating:
|
|
7/31/2025 1:13 PM | |
Joined: 7/24/2025 Last visit: 8/17/2025 Posts: 26 Rating:
|
This is my project and on the lost line I want to display the average between the Mathematical calculation between INPUT - OUTPUT = LOST. At the moment if INPUT or OUTPUT has a value greater than 32K LOST becomes 0AttachmentCircuit Diagram1.zip (44 Downloads) |
Last edited by: Moderator_Lan at: 07/31/2025 13:17:57Text formatting optimized |
|
7/31/2025 1:17 PM | |
Joined: 7/24/2025 Last visit: 8/17/2025 Posts: 26 Rating:
|
Is there any logic that can help me compare values greater than 32,768? |
7/31/2025 1:25 PM | |
Joined: 7/24/2025 Last visit: 8/17/2025 Posts: 26 Rating:
|
Now it's clearer, thanks for the support. |
7/31/2025 1:26 PM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35960 Rating:
|
LOGO! doesn't have any bus blocks for this by default, because LOGO! is designed only for integers.
AttachmentCompare_values_max_999,999,999,999_0BA8.Standard.zip (52 Downloads) |
Follow us on