3/18/2018 10:34 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2984)
|
1.) which D425 with which FW? 2.) Why drive, can you create external encoder in sinamics? |
3/20/2018 1:53 AM | |
Posts: 305 Rating: (1) |
via config ,can read the encoder data ... must use simotion funtion ? |
3/20/2018 6:55 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2984)
|
yes you must |
3/20/2018 7:24 AM | |
Posts: 305 Rating: (1) |
i config encoder at sinamics,connect it to funtion,but restart d425 ,has error . |
3/20/2018 8:02 AM | |
Posts: 305 Rating: (1) |
can you config a example give me test ,i think it is fast idea . eveytime is not right.... |
Last edited by: TechWing at: 3/20/2018 8:34:56 AM |
|
3/20/2018 1:39 PM | |
Posts: 305 Rating: (1) |
hello.i config the funtion to download ,but program has any command ,the D425 can runnng ,program is blank ,D425 can running ,what is wrong ? |
3/20/2018 3:21 PM | |
Posts: 305 Rating: (1) |
use telegram 106 is right ? enable extenal encoder ,r482 not data . |
3/20/2018 4:16 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2984)
|
Hello, no telegram 106 is wrong. Do you have a encoder created so that you can use this commands?
Christoph |
3/21/2018 5:28 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2984)
|
whcih to is configured for the dataexchange in simotion with the drive? |
3/21/2018 7:20 AM | |
Posts: 305 Rating: (1) |
now can connect encoder ,at sinamics read positon data. TO connect it ,can't enable extenalencoder. how can setup TO parameter with SSI... |
3/21/2018 7:31 AM | |
Posts: 305 Rating: (1) |
upload sinamics ? i change TO parameter ,download,the D425 can't change . |
Last edited by: TechWing at: 3/21/2018 7:33:32 AM |
|
3/21/2018 7:42 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2984)
|
D425 can't change cant't change what? |
3/21/2018 7:49 AM | |
Posts: 305 Rating: (1) |
TO can't change encoder about SSI parameter. download and restart ,the data only use default... |
3/22/2018 8:50 AM | |
Posts: 305 Rating: (1) |
the old version is not support the SSI via SMC20 to connect .... |
Follow us on