9/30/2016 8:18 AM | |
Joined: 4/28/2015 Last visit: 5/15/2024 Posts: 3345 Rating: (377)
|
In this topic you can find a document how to create a first project with the Eclipse IDE. After working through this document, the USER LED of the SIMATIC IOT2000 is blinking. Some of the content in this document is related to the "Setting up the SIMATIC IOT2000". Please work through the Setting up at first. Feel free to share your experience! Update 04.02.2020 Updated attached document. Is now related to Image version V2.6 Update 19.04.2017 A new version of the Eclipse PlugIn (V1.2.0) is now available athttps://support.industry.siemens.com/cs/document/109744106/simatic-iot2000-eclipse-plugin?dti=0&lc=de-WW PlugIn runs now within Eclipse Mars and adding C-projects is possible. Download "Eclipse_Plugin_IOT2000_V1.2.0.zip, extract it and copy the .jar file to the dropins folder of your Eclipse directory. Remove the old .jar file in the dropins folder. New Windows SDK (V2.1.3) is available. Update 06.03.2017 A new version of the Eclipse PlugIn (V1.1.0) is now available at https://support.industry.siemens.com/cs/document/109744106/simatic-iot2000-eclipse-plugin?dti=0&lc=de-WW Some fixes are done, for example building errors after adding source files. Download "Eclipse_Plugin_IOT2000_V1.1.0.zip, extract it and copy the .jar file to the dropins folder of your Eclipse directory. Remove the old .jar file in the dropins folder. Update 03.01.2017: Attachment109744106_SIMATIC_IOT2000_Getting_Started.pdf (2955 Downloads) |
Last edited by: bergmanu at: 9/30/2016 9:08:23 AMadded link and document Last edited by: bergmanu at: 9/30/2016 11:43:12 AMedit document Last edited by: IOT2000_Moderator at: 1/3/2017 8:15:49 AMLast edited by: bergmanu at: 3/6/2017 2:49:42 PMnew version of Eclipse PlugIn Last edited by: bergmanu at: 4/7/2017 1:48:55 PMadded hint regarding 7-Zip to document Last edited by: bergmanu at: 4/19/2017 10:07:47 AMLast edited by: bergmanu at: 11/3/2017 1:18:54 PMcorrected screenshot regarding target path Last edited by: bergmanu at: 02/04/2020 14:54:59Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to9 thankful Users |
11/15/2016 2:57 PM | |
Posts: 2 Rating: (0) |
Very interesting. Thanks |
This contribution was helpful to1 thankful Users |
11/28/2016 2:14 PM | |
Posts: 2 Rating: (0) |
Hello All, The Eclipse instance that I have installed is not able to resolve the following code: mraa::Gpio* Is anyone faced this issue?? Many thanks Thibaud |
11/29/2016 8:33 AM | |
Posts: 2 Rating: (0) |
Hi Thanks for you answer. It solved my issue. Regards Thibaud |
1/27/2017 12:36 AM | |
Posts: 30 Rating: (5) |
Hi, I think you're looking for this: http://www.yoctoproject.org/docs/2.1/dev-manual/dev-manual.html#cross-development-toolchain http://www.yoctoproject.org/docs/2.1/sdk-manual/sdk-manual.html |
1/30/2017 2:22 PM | |
Posts: 5 Rating: (0) |
Hi bergmanu, thanks for your fast answer, but it still doesn´t work. In the direction "IOT2000 Release" is nothing to select. |
1/31/2017 11:12 AM | |
Posts: 5 Rating: (0) |
Hi, here is the consoloutput after the build process (attachment). What does the error message mean? |
1/31/2017 11:20 AM | |
Posts: 71 Rating: (16) |
Hello schmidpa, please have a look at this thread: https://support.industry.siemens.com/tf/ww/en/posts/build-error-for-the-example-application/160267/?page=0&pageSize=10 |
2/21/2017 12:59 PM | |
Posts: 71 Rating: (16) |
Unpacking the archives creates links on the file system. Those are not created properly if 7zip is run without administrator rights. |
3/23/2017 8:18 PM | |
Posts: 1 Rating: (0) |
Hello, the example in the Getting Started shows how to programm the IOT2000 with C/C++. Is it also possible to use other languages like C#? |
4/9/2017 7:14 PM | |
Posts: 2 Rating: (2) |
Hello, I installed the Getting Started on my IOT200, too, and want to start my exercises. But I cannot find any documentation how to address the IOs. For example: where is documented, that the USER led is addressed via mrcc with number 13? And where is documented, how to address the USER button? I found the documentation about the mrcc at http://iotdk.intel.com/docs/master/mraa/index.html but I could not find any device specific information there. Best Regards, barteldan2 |
This contribution was helpful to1 thankful Users |
4/11/2017 10:05 AM | |
Joined: 4/28/2015 Last visit: 5/15/2024 Posts: 3345 Rating: (377)
|
Hi, that the USER LED is pin 13 is described in the Getting Started Document. There are several posts about the User Button. For example here: https://support.industry.siemens.com/tf/ww/en/posts/how-can-the-status-of-the-user-button-be-queried/152949/?page=0&pageSize=10 The assignment of the other GPIOs could be found here: or you can use this picture for example. Best regards! |
Last edited by: bergmanu at: 4/11/2017 10:05:40 AMNot working for IOT2050 support anymore from March 1st, 2024. |
|