9/12/2022 9:50 AM | |
Joined: 9/12/2022 Last visit: 8/27/2024 Posts: 10 Rating: (0) |
Hi Stefan, Im using a TP700. And i am currently running on TIA V15.1. Firmware should be V2.6 Best Regards Magnus |
9/12/2022 10:02 AM | |
Joined: 1/21/2013 Last visit: 9/13/2024 Posts: 3096 Rating: (483)
|
Hi Magnus, please check your transfer settings. The transfer channel should be set to PN/IE. Kind regards |
9/12/2022 11:15 AM | |
Joined: 9/12/2022 Last visit: 8/27/2024 Posts: 10 Rating: (0) |
Hi Stefan, I use this, and as you can see I am not able to see anything besides the PLC. Best regards Magnus |
9/19/2022 1:31 PM | |
Joined: 8/3/2009 Last visit: 9/13/2024 Posts: 13684 Rating: (1726) |
Hello If you want to load something to the Panel you should work with Extended Download to device. If you then want to use PN_IE to download then you also have to use the PN_IE in the trensfer settings of the Panel. if you use ethernet here then you cannot find the Panel. Check also this FAQs: https://support.industry.siemens.com/cs/ww/en/view/58522603 https://support.industry.siemens.com/cs/ww/en/view/88633853 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on