1/21/2025 12:18 PM | |
Joined: 12/23/2024 Last visit: 1/22/2025 Posts: 1 Rating:
|
Hello I am using a delta HMI to receive a mobile number with 12 digits and then use it with GSM module to send messages to. Since my phone number has 12 digits, I am using QWORD as the data type in HMI. However, I can't convert it to string in PLC. What should I do? |
1/22/2025 3:01 PM | |
Joined: 8/3/2009 Last visit: 2/21/2025 Posts: 14801 Rating:
|
Hello AutoGen_9530526 So do you have reached getting the value into the PLC? which Datatype do you use ini the PLC DB for this? I do not know which datatypes the third party HMI supports for the PLc communication? do you have a list for us? Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on