2/2/2016 2:26 PM | |
Joined: 8/13/2015 Last visit: 11/12/2024 Posts: 85 Rating: (6) |
Hello all, I have the same problem with one laptop (tia portal v13 sp1 upd6). No accessible devices on network. Other laptop (v13 sp1 upd5) - all fine. Bigest difference I see in PG/PC interface is SIMATIC Device Driver 09.00.06.02_01.01.00.02 vs 09.00.06.02_01.01.00.01 and SIMATIC Device Driver WOW 29.00.06.02_01.01.00.02 vs 29.00.06.02_01.01.00.01 02 - no access. Reinstaled network drivers, connected through router - no success. A month ago all worked fine. With the same CPU's. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/4/2016 11:12:51 AMNew subject after splitting |
|
2/4/2016 2:09 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
For months I had on and off problems connecting and at times I was locked out of the entire day and spent hours upon hours trying and usually when I connected back on I had no idea of what the problem was. I uninstalled anti-virus software and firewall and did many system restores and sometimes it worked and sometimes not. A week ago or so I spent an entire day doing everything I could to find the root of the problem and whenever Ii thought I knew what it was I recreated it and to confirm that I knew what the problem was.
Attachmentconnection_problems1.pdf (526 Downloads) |
2/4/2016 2:12 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Attachment too large I had to split it up.Attachmentconnection_problems2.pdf (519 Downloads) |
Follow us on