2/18/2019 7:11 PM | |
Joined: 4/8/2013 Last visit: 9/20/2023 Posts: 5 Rating: (0) |
Hello to everyone, i have a problem with PLCSIM advanced with Mode Virtual Eth. Adapter. i need to test a my application with opc ua communication. My problem is to download the configuration on TIA Portal V15, when i try to found accessible device, but no one appared. I try with Proneta to find on Virtual Eht. Adapter but no one device come out on list. I know my version of windows 10 pro (1809) is not listed in supported os, and i run the application with administrative privilege, and checked the option of "Siemens PLCSIM Virtual Switch" is setted only on my NIC. the configuration is:
What is the problem? Thank you in advaice for the support AttachmentPlcsim problem.zip (91 Downloads) |
2/19/2019 4:07 PM | |
Joined: 10/10/2005 Last visit: 8/29/2024 Posts: 1917 Rating: (136) |
Hello Roland88, is there also an online connection to a real CPU? In this case avoid both connection and disconnect the real online connection, so that you have only the connection with PLCSIM Advanced. Have you know-how-protected blocks in your project? Most likely the option "Can be simulated with S7-PLCSIM Advanced" has not been enabled for these blocks. Further informations you will find in the FAQ (link): https://support.industry.siemens.com/cs/ww/en/view/109754928 Other reason are not enough space of the swap file. Check the settings of the virtual memory in System Properties of your operating system. The Windows operating systems supported require additional memory on the hard disk (typically disk C:) for the swap file, depending on the memory expansion available. You should keep at least twice the size of the main memory free. With best regardsCicero |
This contribution was helpful to1 thankful Users |
Follow us on