9/8/2019 9:55 PM | |
Posts: 2 Rating: (0) |
Similar problem. The PLC is CPU 1517F-S PN/DP, HMI is KTP900 Mobile. What I did: 1. Running PLC simulation and RunTime: - change PC/PG interface settings for STEP7 and for WinCC to all PLCSIM points ( local, TCPIP, Profibus, ISO ... ) - HMI introduced to PLC project and configured connection to local ProfiNet 2. Running PLC simulation and HMI simulation - the same as above; - changed HMI device to the panel with Profibus and connected the HMI to PLC ProfiBus. - configured connection via Profibus, CPU master address2, HMI slave address 1 The best result is online diagnostic says that the HMI is not accessible or reachable. Didn't appeared in available nodes list. The confguration works on hardware: no HMI device in PLC project. Connected via ProfiNet. HMI communication settings a single connection via S7Online on ProfiNet. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/09/2019 07:15:13New subject after splitting |
|
Follow us on