1/27/2016 8:38 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi, searching for accessible nodes is a MAC-Adress-Broadcast. Some antivirus-programms are blocking it with a function called like "Network-Protect" or similar. Try to disable this function or the whole anti-virus-scan. Maybe an other device in your network is blocking that function(switch, router). you can also try to install the SIMATIC Automation Tool. Whit this Tool you will also install PC-Identifier-SW, that repairs the programming interfaces. hope this helps. regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
1/27/2016 11:05 AM | |
Joined: 1/17/2013 Last visit: 5/3/2024 Posts: 136 Rating: (23) |
Thanks guys i'm gonna try to disable the antivirus as soon as possible then i'll provide a feedback post |
1/27/2016 11:35 AM | |
Joined: 10/2/2013 Last visit: 9/30/2024 Posts: 339 Rating: (52) |
please check once any type of error in SET PG/PC Diagnostic as shown attached check also in siemens communication setting, I hope this may help you Attachmentforum.rar (657 Downloads) |
Technology is best when it brings people together,so we are here now :) |
|
This contribution was helpful to1 thankful Users |
11/13/2017 10:51 AM | |
Posts: 8 Rating: (0) |
Run again SIMATIC PnDiscovery Service |
Follow us on