9/28/2016 3:08 PM | |
Posts: 11 Rating: (0) |
Hi there! I have same problem, but can not find any solution. My PC after install of Safety basic pack (not sure it is the real reason) is not able to detect any accesible nodes. I can now ping, go online and completly work with old CPUs (S7-1211 or S7-1512) where I know theirs IPs, but I am not able to connect to new one (S7-1214FC 6ES7214-1AF40-0XB0), which has still no IP set. In all cases of different CPUs connected no accesible nodes found. I use direct connection from my LAN to CPU. Green LINK LED lit, yellow Rx/Tx LED flashes irregularly all the time. Different cables tested (UTP, STP, green ProfiNet 2×2, direct and cross), same result. I switch off antivirus SW (Avast) and check services list. There are from Siemens only two services "S7DOS help service" and "SIMATIC Trace Service", both looks running. I use Win7 Ultimate x64 with direct install (no Virtual PC) of SIMATIC STEP 7 Professional V13.0 SP1 update 9 and SIMATIC STEP 7 Safety V13 SP1 update 5. Thanks for any idea ;) ------------------------------------------------------------------------------------------ |
Last edited by: RhinoCZ at: 9/28/2016 3:21:07 PMLast edited by: Min_Moderator at: 9/29/2016 12:53:01 PMNew subject after splitting |
|
9/28/2016 7:42 PM | |
Posts: 2 Rating: (0) |
one more attachment. |
9/29/2016 7:07 AM | |
Joined: 5/12/2006 Last visit: 9/27/2024 Posts: 22376 Rating: (3015)
|
Hello, or try to installSiemens Automation Toolit contains a newer Version of communication drivers a can be solved the problem with the PG/PC Interface.
|
Last edited by: ChristophD at: 9/29/2016 7:07:42 AM |
|
Follow us on