3/18/2022 1:44 PM | |
Joined: 8/3/2009 Last visit: 8/15/2024 Posts: 13561 Rating:
|
Hello does this work on a Panel?? I think not, this should only have a chance on a PC based Rutnime System. What should work is to use the startprogram systemfunction with a cmd command and the ping as parameter and also a redirection of the output to a file (>) linke in DOS. then you have to wait a second or so in the script and then you can readout the file with the script API (LINK) functions and check if the Ping result was OK. Its a quite indirect workaround but it sould work. I used it in the past for other DOS commands on a Comfort Panel. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on