6/8/2023 10:21 AM | |
Joined: 7/19/2022 Last visit: 9/16/2025 Posts: 436 Rating:
|
Hello AutoGen_2379618, The parameter for the torque value is r31 in V90. This value can be transferred to the PLC via acyclic communication: SINAMICS V: Acyclic communication between SIMATIC S7-1500 and SINAMICS V90 via PROFINET As for the torque limits; they cannot be written to the TO on an S7-1200. Only possible via V90 GSDML and additional telegram 750 (M_LIMIT_POS, M_LIMIT_NEG, M_ACT): SINAMICS V90 PROFINET, SIMOTICS S-1FL6 Operating Instructions |
If this Information really helps, you could use the Rate function |
|
Follow us on