12/14/2023 1:23 PM | |
Joined: 10/3/2021 Last visit: 4/26/2025 Posts: 2 Rating:
|
Hi Ixo65 I saw that you are interested about HSP files. I need your help about hsp0185 v 3.0 v90. I am using TIA Portal v19. I have a project from TIA V17. When I try to upgrade the project from v17 to v19 I am taking error about that hsp0185 v90 v3.0 installation requires. I installed last HSP verison for V19. But there was no HSP0185 in that. I am sharing the screen image for you see Can you share ıf you have hsp0185 for TIA V19 or can you help me if you can do anything ? Have a nice day. ------------------------------------------------------------------------------------------ |
Last edited by: grhntrmn at: 12/14/2023 13:24:41Last edited by: The Helping Hand at: 12/14/2023 13:30:56New subject after splitting. |
|
12/14/2023 1:27 PM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35964 Rating:
|
Take a look at this topic: Need HSP0185 SINAMICS V90 PN V3.0 |
12/14/2023 2:21 PM | |
Joined: 8/21/2014 Last visit: 9/12/2025 Posts: 1087 Rating:
|
Closed cause question posted twice. The second thread with the subject Need HSP0185 SINAMICS V90 PN V3.0 is published within the conference STEP 7 (TIA Portal) Best regards, |
My Forum is the place to personalize your profile, |
|
Follow us on