12/23/2023 7:25 PM | |
Joined: 9/27/2006 Last visit: 11/4/2024 Posts: 12293 Rating: (2690) |
Hello viren; Siemens has tasked Siemens India to produce a line of PLCs amd HMIs for the South-Asian market, they deveopped the S7-200 Smart CPus and the smart line HMIs. They are designed with interfaces that make connecting them to each other very easy, which is not the case with other Siemens automation families, such as the S7-1200.. Our friend qwazee has sumarized the connection possibilities of a Smart line 700 with a S7-1200 CPU in the following thread: https://support.industry.siemens.com/forum/ca/en/posts/smart-line-700-v3-and-s7-1200/289053 Sorry, it is not possible to work witth a s7-1200 PLC and a Smartline HMI.directly. Unless you look at the alternative of adding a CM 1241 (6ES7241-1CH32-0XB0) RS422-RS485 serial communication module to the S7-1200 and use the integrated Modbus RTU instructions of TIA Portal to program your exchanges with the HMI, which would be a lot of work. Hope this helps, |
This contribution was helpful to1 thankful Users |
Follow us on