7/24/2024 6:29 PM | |
Joined: 8/6/2018 Last visit: 7/24/2024 Posts: 3 Rating: (0) |
I have used 6ES7 132-6BD20-0DA0 card having High Speed Output with Siemens S7-1512 PLC & Remote Card IM 155-6 PN/2 HF. Detail of the Card DQ 4x24VDC/2A HS : Digital output module DQ4 x 24VDC / 2A HS; four operating modes: DQ HS, pulse width modulation, oversampling, cam controller; value status; configurable diagnostics; substitute value for output; supports PROFIenergy; isochronous mode; Module to Module communication (MtM) Can I use this Card to Control 3 No of Stepper Motors ? ------------------------------------------------------------------------------------------ |
Last edited by: Wit_Moderator at: 07/25/2024 07:51:30New subject after splitting |
|
Follow us on