1/12/2022 5:47 PM | |
Joined: 8/28/2012 Last visit: 7/4/2024 Posts: 9 Rating: (0) |
Hello, I would like to read out the parameters of a Sinamics drive with a IOT2050/ Node red. I can read them out if I use a 1200 or 1500 plc in between and put the parameters in to a datablock of the PLC, but I would like to read them out without a PLC. I don't know what protocol to use when I don't use a PLC in between. Can somebody help me, all tips and idea's are very welcome. Kind regards, Frits van schagen Attachmentflows_txt_is_Json.TXT (459 Downloads) |
1/17/2022 4:46 AM | |
Joined: 5/19/2006 Last visit: 9/5/2024 Posts: 548 Rating: (107) |
Besides the native mode of accessing the parameters via DRIVEESANY syntax (STARTER, Startdrive, Drive ES, Simotion Scout), it looks like from FW 4.7 or so Sinamics drives map the parameters to DB blocks see Application example 109481157 Attached I am reading r26 "DC link voltage smoothed" from a G120 Drive using address DB26.DBD0 that in Node red syntax is DB26,R0. |
Last edited by: Jen_Moderator at: 01/17/2022 07:23:37Optimized link. |
|
This contribution was helpful to1 thankful Users |
9/4/2024 10:32 AM | |
Joined: 7/30/2024 Last visit: 9/6/2024 Posts: 134 Rating: (3) |
New question published by AutoGen_8022241 is split to a separate thread with the subject S120-CU320PN_2: read the parameters with Node-Red. Best regards |
Follow us on