10/15/2024 11:29 AM | |
Joined: 9/27/2023 Last visit: 10/15/2024 Posts: 1 Rating: (0) |
Hello, I am currently using the Honeywell PX6i printer configured via TCP/IP to my S7-1516-3 PN/DP. As a protocol of keeping the spare, I am advised to upgrade it to PX65. Can i swap the printer with the same IP address or do i have to change the Hardware and Software address for the same in order to get the data with same length of addresses used. Kindly suggest. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/15/2024 11:40:42New subject after splitting |
|
Follow us on