2/12/2025 9:36 AM | |
Joined: 9/30/2016 Last visit: 8/13/2025 Posts: 946 Rating:
|
Please also see the attached screenshots. We have a machine where I am missing an "enabled" signal on the WinCC display. With WinCC Graphics Designer I can see that the status bits bits shown on the popup in case are: Høj - DrejeskiveHastighedStatus Bit 0 Lav - DrejeskiveHastighedStatus Bit 0 Enable - DrejeskiveHastighedStatus Bit 9 Fejl - DrejeskiveHastighedStatus Bit 8 This means that the bit I need to make the enabled signal green is "DrejeskiveHastighedStatus" Bit 9 With the Tag Management I can see that address for "DrejeskiveHastighedStatus" is DB2002.DBW26. Opening DB2002 I can see that DBX26.1 is named .Enable but searching for this bit as well as searching for DB2002.DBW26 in the PLC logic finds nothing. When I seach for DB2002 I find a few places that PLC logic is writing to this DB but not to DBW26. So - where and how is bit 9 in DB2002.DBW26 set and how do I find it (also for other signals in the future)? AttachmentGH24.zip (164 Downloads) |
Follow us on