8/22/2025 8:45 AM | |
Joined: 8/20/2024 Last visit: 8/22/2025 Posts: 1 Rating:
|
TIA V19 Update3 WinCC Basic/Comfort/Advanced V19 Update 3 WinCC Professional V19 Update3 WinCC Unified v19 update 3 MTP1500 Unified Comfort V19.00.00.03_05.04.00.01 Scada V19.4
I have tested this ************************************************************************************** To resolve the issue of collaboration between a Siemens WinCC Unified Comfort Panel and a WinCC Unified SCADA server, you can follow these steps:
By following these steps, you should be able to establish a successful collaboration between the Siemens WinCC Unified Comfort Panel and the WinCC Unified SCADA server. Sources:
*********************************************************************************** I get this log information from the trace tool when I have added the certificate on panel and Scada 280(0x30f8) Failed to load Operational Certificate, peer name: XXX.XXX.XXX.XXX:49680 8700 (0x3458) Failed to load Operational Certificate, No OC found for peer. I also get a alarm message in the panel If I remove the certificate I get no log messages on the trace.
Best regards Henrik Andersson
|
9/3/2025 11:09 AM | |
Joined: 8/3/2009 Last visit: 9/17/2025 Posts: 16447 Rating:
|
Hello henrik_andersson58 If you have already followed the steps in this example Step By Step and I does not work: https://support.industry.siemens.com/cs/ww/en/view/109896068 then it would be also possible to open a Service Request at Siemens Support Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on