9/30/2009 9:59 PM | |
Joined: 9/6/2008 Last visit: 3/29/2024 Posts: 134 Rating: (16) |
corect me if i dont understund but it look that you had a trial or demo (whatever) version and you buy one upgrade cd and not a complete version? whell it looks like you spend some money . with this cd you are able to upgrade to v6.x only if you have the valid (full) earlier version . not a trial-demo one. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objID=10805245&subtype=133100 Description: The current upgrade for LOGO!Soft Comfort, which enables you to update your earlier version to the current version, is available to download at the following Internet address: http://www.automation.siemens.com/logo/html_00/support/01ToolsDownloads/index.html This upgrade is also available on CD. MLFB: 6ED1058-0CA02-0YE0 |
http://electrotech-techblogg.blogspot.gr/ |
|
10/1/2009 1:16 PM | |
Posts: 16 Rating: (2) |
My mistake. I thought that was what the upgrade was for, to upgrade a free-trial version to a full version. Oh, well .... |
10/5/2009 9:56 PM | |
Posts: 7 Rating: (0) |
See Window - Options - Interface and try to find connection. But first of all you need to install Driver for USB PC Cable: |
Follow us on