1/21/2010 9:45 AM | |
Posts: 3609 Rating: (29) |
Import of a Technical Question of an User 256 wrote: Dear I have a faulty OP17DP and now i want to replace this OP17DP with a new OP17PP.but there is a problem that OP17DP has a profibus provision and OP17PP has no profibus provision.so can u help me to install OP17PP in the replacement of OP17DP. Regrads |
1/26/2010 6:30 AM | |
Joined: 9/28/2007 Last visit: 2/20/2024 Posts: 234 Rating: (12) |
I have orignal protool project.Plc is S7 which i want to interface. |
Muhammad Munir |
|
Follow us on