2/6/2010 2:23 PM | |
Joined: 8/12/2009 Last visit: 10/25/2023 Posts: 27 Rating:
|
Hello, I want to connect a Festo CPX - FB13 island via ProfiBus to a Panel PC 477B. I set up the configuration(input and output modules), but i still have problems with ProfiBus communication. On the festo node the bus failer led(red) is blinking and on panel pc, in WinLC RTX interface EXTF led is red and BUSF1 led is blinking too. I attach this simple project and i hope somebody can help me. The project is make in Step7. Thank You.
Attachment3_feb_Testconf_1.zip (562 Downloads) |
Follow us on