2/10/2010 7:38 AM | |
Posts: 3609 Rating:
|
Import of a Technical Question of an User Javieron wrote: Any body can help me, I need a example to read modbus parameters in s7-1200 from flowmeter MAG 5100W , I need to read TOTALIZER 1, TOTALIZER 2 AND Absolute Volumeflow, right now I can read the Adress slave number, the TAG "flowmeter", The Baud rate, only. |
Follow us on