7/21/2011 11:16 AM | |
Joined: 5/4/2009 Last visit: 5/28/2024 Posts: 914 Rating: (40) |
Yes my dear CPU314C-2DP... |
Aim Higher |
|
7/21/2011 11:22 AM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Info - http://support.automation.siemens.com/WW/view/en/23657941 |
7/21/2011 11:52 AM | |
Joined: 4/24/2006 Last visit: 10/14/2024 Posts: 8745 Rating: (1168) |
Dear Tomy, Please have a look at edit notes in my first post. Perhaps it is useful Best regards, Wizard |
7/21/2011 11:59 AM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
So, all the settings should be done in hardware configuration as Wizard already mentioned. Look at attachment. And you can use http://support.automation.siemens.com/WW/view/en/18467424In OB40 you can specify logic after its calling what to do after...UseStep7' help concerning OB40... Best regards, Hristo Mihalev |
7/21/2011 12:21 PM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Above mentioned CPU is not support OB41. Check it in hardware configuration. |
This contribution was helpful to1 thankful Users |
Follow us on