2/2/2012 10:46 AM | |
Posts: 206 Rating: (22) |
Hello bhole, excuse the the late answer. The problem you have, might be caused by the data record communication. This is done witn SFC58/59 or SFB 52/53 there is a FAQ for this matter. http://support.automation.siemens.com/WW/view/en/32210587 You can try not to activate all SFC/SFB calls at the same time, e.g. 100ms for channel 1 and other 100ms the 2. channel. Can you tell me what the order no. of the Siwarex is? How many Siwarex U do you have in your installation? Do you use SFC calls or our FB for the new Siwarex U 7MH4950*? Regards ABenno |
2/14/2012 1:01 PM | |
Posts: 206 Rating: (22) |
Hello Bhole11, if you have problems with handling the SFC. Ther would be also the possibility to use the I/O mode of the Siwarex U. Have a look to the FAQ http://support.automation.siemens.com/WW/view/en/17167112 Regards ABenno |
Follow us on