3/5/2012 12:15 PM | |
Joined: 7/28/2009 Last visit: 5/10/2022 Posts: 90 Rating: (7) |
Dear Manfred That was a very detailed explanation. Thank you very much. I just want to know whether we can insert a USB Stick as a part of external memory device rather than going for a MMC. Please reply as one of my customer requires this in his site. Regards Revathy |
Last edited by: O_Moderator at: 3/5/2012 1:52 PMnew subject after splitting from /tf/WW/en/Posts/33701#top Cheers |
|
3/5/2012 3:16 PM | |
Posts: 3037 Rating: (192)
|
Hello, Which panel do you use? When you use an OP77B, then you can not use an USB Stick. This is not possible for this panel. You must use a MMC card. You can see more information about external memory in the following link. Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have? Tweety |
Follow us on