5/3/2008 8:03 AM | |
Posts: 148 Rating: (11) |
I think the FAQ should be inserted on the main screen it self. |
5/3/2008 8:22 AM | |
Posts: 2661 Rating: (279) |
tambe: What exactly do you mean by this? Can you explain some more? Regards |
11/29/2011 11:02 AM | |
Posts: 378 Rating: (47) |
Hello, there are many ways to find faqs. Here two possibilities: 1. Use the search-field on the upper right corner in the forum window. After reaching to the results you have to click on faq (result can be found here) 2. Use the search field on the starting-support-page ...... Best regards Bilao |
This contribution was helpful to1 thankful Users |
3/8/2012 2:19 PM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191) |
I have also a way, with which you find only FAQs: 1. Go to Prodcut Support (in the menue) 2. Open the Product Tree on the left side 3. Then selectin this tree e.g. for PCS 7"Product Information" -> "Automation Technology" -> "SIMATIC PCS 7" 4. Now, click the register "Entry List" and select in the Pull Down List "FAQ". 5. If you write a catchword in the search line, then you will get all the FAQs for PCS 7 for that catchword. Regards |
Last edited by: Thunderstorm at: 3/8/2012 2:43 PMSIMATIC PCS 7 - Overview |
|
Follow us on