4/10/2012 9:43 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello, To make a upload there: 1. using a WinCC Flex -Uploading only possible, if the Transfer of the current project file from the configuration computer to the operating unit mustbe performed using the Upload option "Enable backtransfer". 2. using a Prosave - after is possible to make restore only into the same type of panel. Cables to do that: 1.RS232/PPIMulti-Master- cable 2.USB/PPI cable(6ES7 901-3DB30-0XA0) 3. Ethernet 4. USB(Host-to-Host) More info atProjecttransferandSIMATIC HMI HMI device MP 277 Best regards, Hristo Mihalev
|
This contribution was helpful to2 thankful Users |
4/11/2012 11:08 AM | |
Joined: 9/14/2009 Last visit: 12/7/2023 Posts: 41 Rating: (0) |
Dearpoya_xp Regards,
|
Last edited by: esem2704 at: 4/11/2012 11:10 AM |
|
Follow us on