4/22/2012 4:40 PM | |
Posts: 8946 Rating:
|
You have to use an isolation monitor. |
4/25/2012 12:17 PM | |
Posts: 58 Rating:
|
Dear Shahid, The isolation monitor from Bender can be used for ground fault monitoring. It gives alarm and trip contact according to the insulation values set by the user (insulation between ground and phase in kOhm or MOhm). These changeover contacts can be taken into CU as DI and then can be used as wished. Please refer to the attachment for the bender relay information. Regards Ajay Gupta AttachmentINSULATION MONITOR.PDF (551 Downloads) |
Follow us on