1/11/2012 4:51 PM | |
Joined: 4/24/2006 Last visit: 10/3/2024 Posts: 8744 Rating: (1168)
|
Hello, I have found this link: Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP? (Perhaps it might help) Best regards, Wizard |
This contribution was helpful to1 thankful Users |
1/11/2012 5:15 PM | |
Posts: 6 Rating: (0) |
Wizard, Thank you very much for the quick reply and excellent answer. That helps a lot. Kind regards, Richard. |
This contribution was helpful to1 thankful Users |
7/23/2012 3:15 PM | |
Posts: 3037 Rating: (192)
|
Hello Enia, You can use 6 connection of PLC at MP377. You have one access point at MP377. You can use connection about Profibus or about ethernet. You can not use both on a MP377. You can use both at the PC Runtime. See the following FAQ. Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP? Tweety |
Follow us on