4/2/2013 7:45 AM | |
Posts: 197 Rating: (3) |
@ hdhosseini : "2- "LAR1 P#DBX.0 " is a wrong notation for STL editor and you should try "LAR1 P#DBX0.0 " Yes, I got it. It was actually a copy-paste error .......in a rush last night when I copied / posted those codes. Never the less, my point was to check if: LAR1 P#DBX0.0 LAR2 P#DBX0.0 and then L B [AR1,P#0.0] T B [AR2,P#0.0] will work or not (in line with the originality of the first post)? And apparently, from your reply, it seems it isgood and ok .... ofcourse with increasing the length of the array of the DB from 9 to 18. Regards |
Follow us on