8/13/2013 11:10 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Moderator For sure they already detected that. It will be good if you receive two premiums. I hope you didn't use different names in forum and because of that send two times the same address. This is joke only! Best regards, Hristo Mihalev
|
8/13/2013 11:13 AM | |
Joined: 9/1/2005 Last visit: 9/18/2024 Posts: 4104 Rating: (195) |
Hello DS SURESH KUMAR, I'm sorry for the delay I'm a little bit busy at the moment. I have checked the entries. Yes there are too but with the same information. So we will ignore one of them. We are still waiting for the contact data of some of the winners. But I hope we could forward the addresses to our logistic partner at the end of the next week. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
8/13/2013 11:40 AM | |
Joined: 4/17/2012 Last visit: 8/30/2024 Posts: 474 Rating: (10) |
Hi, When i filled first time i didn't received any successfull completion message at the last step . So once again i filled the form Hope u understand
|
Follow us on