6/20/2012 2:09 AM | |
Posts: 17 Rating:
|
MS can do this,as far as I know . |
6/20/2012 6:52 PM | |
Posts: 151 Rating:
|
Hi thanozn, You are right, BW100/BW500 are intended as integrators for belt weighers. About the choice of weighframe, I would contact a company who build complete weighframes for these applications. As far as I know, Siemens only builds weigh frames for a continuous flow of material on the belt, not to weigh separate bags. The siwarex FTA has different preprogrammed applications. I would base my choice on the PLC platform you are planning to use, and the ease of programming. If you can avoid writing a complete PLC program by using one of the preprogrammed applications in the siwarex module, this saves you a lot of time for programming, testing and troubleshooting! "Check" also http://www.automation.siemens.com/w1/automation-technology-checkweighing-20891.htm Best Regards, SonicRanger. |
8/27/2013 11:15 PM | |
Joined: 4/21/2006 Last visit: 7/5/2024 Posts: 510 Rating:
|
New question was transferred to a new thread: siwarex wp231 the s7-1200 compactable weighing module for the same check weigher application |
Follow us on