4/10/2014 2:34 PM | |
Joined: 4/11/2011 Last visit: 6/17/2024 Posts: 132 Rating:
|
First of all: - what kind of material (fluid, solid) - maximum weight of weighed material - maximum weight of tare and weighing platform (if used) - required accuracy in kg - sampling time (time between two measurements to calculate flow rate) If you have weighing platform: - what kind of weighing platform is used (one or four load cells) - sensing range (maximum) and sensitivity in mV/V of load cell(s) Do you have weighing electronics? - for 1200 is designed weighing module SIWAREX WP 231. Quite powerfull and very high accuracy. But you need software also (not freeware). - if you want cheaper solution, then you need load cell converter (for example thisor this orfrom here) with analog output 4..20mA and S7 1200 analog signal module 4..20mA. Depends on reguired accuracy but i think SM1231 16bit is ok. Onboard 0..10V analog inputs are 10bit and not very suitable for this application.
|
I'm just a human. Mistakes are allowed. |
|
Follow us on