10/18/2013 10:24 AM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (41) |
Hi janbar_k, to 1) Yes, it is possible. Have a look on this FAQ: http://support.automation.siemens.com/WW/view/de/23842653 to 2a) As I know, it is not possible to integrated a Comfort Panel in a PCS7 project to 2b) It is possible to show process tags from the PCS7 project on the Comfort Panel to 3) Yes, the software is SIMATIC WinCC Comfort (TIA Portal) the HMI Card can you use to backup your project No runtime licencse, only if you want to use the SM@RTservices for remote access to 4)I am not sure, if this is possible. to 5) This is not possible to have the same picture from PCS7 on a Comfort Panel. regards, healthcheck |
Last edited by: Healthcheck at: 10/18/2013 10:25 AMGrundkurs/Systemkurs WinCC V7: |
|
5/22/2014 11:34 AM | |
Joined: 4/21/2006 Last visit: 9/23/2024 Posts: 510 Rating: (24) |
New question was splitted to a new thread: HMI 15" ICP577C Panel PC and S7-400H |
Follow us on