9/28/2014 7:21 AM | |
Joined: 5/28/2008 Last visit: 7/4/2024 Posts: 4510 Rating: (837) |
Hello, As this type of panels are too old, so there is a serial cable to download projects to this panel through PC com port. The serial cable have part number "6XV1 440 - 2K x ab" You can made your own cable if you follow connections (pin assignment) here: You can not use it via COM-USB converter. According to this FAQ "Which connector cables are available for connecting to SIMATIC Panels?", it is stated clearly:
Hope this helps.
|
Ayman Elotaify |
|
This contribution was helpful to2 thankful Users |
9/28/2014 7:48 AM | |
Posts: 3 Rating: (0) |
I made this cable myself. See attachment
|
Last edited by: Peter999 at: 9/28/2014 7:58 AMWrong picture sent first time |
|
Follow us on