8/5/2008 9:34 AM | |
Posts: 2348 Rating: (263) |
What scheme do you use for 4-20 mA (4w/2w)? Is 4-20 obligatory or you can change it to 0-20 for example? |
8/5/2008 5:55 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1425) |
Hi, take a look at the manual of s7-300 modules (http://support.automation.siemens.com/BR/view/en/8859629 ) at the page 292 -297. It has the connection diagram for each type of use. Note the both channels are equally configured. |
Denilson Pegaia |
|
8/6/2008 1:26 AM | |
Posts: 2 Rating: (0) |
Hi, i) I use the 4w scheme and i require only 4 - 20 mA inputs. ii) Thanks for the link to the documentation |
Last edited by: viki1967 at: 8/6/2008 1:28 AM |
|
5/19/2015 1:58 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
Follow us on